Hi,
I have a POE supply design based on the evalboard . The TL432 is used in the feedback loop of the converter.
The design seemed fine until I noticed some drifting in the outpout voltage of the converter. Target voltage was 12.3V and I measured some design at 15.9V.
When investigating the issue, I noticed when changing the TL432, the output voltage was drifting a lot : from 13.2V to 15.9V (with a target voltage of 12.3V).
From the original design provided by OnSemi, the values of the following resistor have changed :
- Rfb3 = 8.2KOhms
- Rbias2 = 1MOhms
Even with changing these values, I should have a current > 1mA on the TL432's cathode, hence i should be in the Recommended operating conditions [1mA ; 100mA], and don't understand why I have so much drifting in my output voltage.
Is this a known issue ?
Is there a mean to minimize the drift from one component to another ?
Regards,
Maxime