This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616: Change charging temperature from 0-60 to 10-45

Part Number: BQ24616

Hi, 
Customer wants to change charging profile, but not change IC. 

Charging temperature should follow IEC62133, or at least charging should be enabled between 10-45 degrees celcius.

I am a bit confused about the bqstroller calculation tools_V1.5

Especially the 70,7 % and the 48,00 % 
- Are these figures connected to the temperature range? and should they be adjusted somehow when changing charging temperatures to 10-45 (from 0-60?)
- These figures do not change when plotting new R_COLD and R_HOT resistance values, this the VCOOL & VWARM parameters don't change either. 

How do i correctly design 10-45 charging with this IC?

Plotting resistance values for 10-45 gives these R-values. Can you confirm that this is correct? - because the VCOOl and VWARM are the same as for 0-60.