Please indicate where best to connect the N.C pins (i.e, pins 1-7, 11, 16 and 21) on the VQFN-24 package.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please indicate where best to connect the N.C pins (i.e, pins 1-7, 11, 16 and 21) on the VQFN-24 package.
Hi Bob,
NC pins of TPS2640 device can be left open or can be connected to RTN for enhanced thermal performance. For VQFN-24 package, NC pins 1-7 & 16 are connected to RTN as it helps to extend the copper area. We left other NC pins OPEN as connecting them to RTN does not make noticeable difference.
Please refer EVM schematic and layout
Best Regards
Rakesh
I did notice the EVM layout yet most read NC as No Connection should be made, and unclear what to do. Please add your suggestions to the datasheet for others. thanks, Bob
Noted Bob. we will include the information in next data sheet revision.
Thanks,
Rakesh