Hi Team,
I'm testing TPS65988EVM with FTDI on board and I follow up user guide below:
- Switch S3 is default setting
- GUI: 6.1.4
- FW: f707.10.10
- Sweep I2C is correct
- Test I2C address is correct
- It also can flash from project successfully
- The debug mode can also shows connected
But! All the registers showed Uninitialized!
I also tried use Aardvark tool with EVM board and customer's board, result are the same! All the connect and flash is correct, but the register in debug mode shows Uninitialized!
Then I tried Dell GUI 6.6.4 with below setting, you can see the debug mode is correct and I can see the register values.
This is very urgent and customer called me several times every day!
Looking forward to your quick support soon!
Thank you!
Marc