This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53659: Schematic Review: TPS53659 for Intel Xeon D-1746 Idaville

Part Number: TPS53659
Other Parts Discussed in Thread: TPS53622

Hi,

As I have mentioned in our earlier chat that We have used TPS53659 & TPS53622 Voltage Regulators with Intel Xeon Processor D-1746TER (Idaville, Brighton City).

You are requested to review the schematic for the same. Here I am sharing the schematic section on VCCIN and V1P80 Supply. 

The Operating conditions are- 

CHANNEL-A
VCCIN_1V8
VID- 1.8V
VBOOT- 1.8V
SVID RANGE- 1.5V to 2V
ICC_TDC- 39A
ICC_MAX- 102A
PHASE- 3
SVID- 0x00
DC TOLERANCE- 0.5%
RIPPLE- 6mV

CHANNEL-B
P1V8_AUX
VBOOT- 1.8V
SVID RANGE- STATIC
ICC_TDC- 1.6A
ICC_MAX- 2A
PHASE- 1
SVID- 0x01
DC TOLERANCE- 0.5%
RIPPLE- 6mV

Please find the attached pdf file (schematic) for the reference and mention the review points. 

VCCIN_TI.pdf

Thank You 

Raj Kumar