This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3890-Q1: a supervisor or pushbutton controller

Part Number: TPS3890-Q1
Other Parts Discussed in Thread: TPS3899

Hi,

I am looking for a supervisor or pushbutton controller that has a programmable output delay and monitoring input setup time.

Specifically, I am looking for a device that can monitor the /MR Setup Delay, which means that the output /Reset signal will only be triggered if the input /MR signal stays low for longer than Tsu.

TPS3890-Q1 triggers the /Reset signal based only on monitoring the voltage of the /MR and /Sense signals.

Thanks

Vitaliy