This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562200: Need Support for RE test issue resolution

Part Number: TPS562200
Other Parts Discussed in Thread: TLV62568

Hello,

We need help here to solve RE testing failure issue.

We are doing RE test in one of the project and we are facing RE failure issue since long time and we have tried multiple iterations to solve it but still we do not have that much significant improvements.
Please see below details of our design.
We do have following board structure.
1)  Main Board which has Sigma Star SoC and  - Connected to Camera Board using PVC cable
2) Camera board has Image sensor Sony iMX335  - Connected to Main Board using PVC cable 
3) we do have separate SD card board - Connected to Main board using Flex cable
4) one is IR LED board - connected to main board using ribbon cable
Camera MCLK is 37 MHz, MIPI is on 594 MHz and SD card frequency is 40 MHz. 
Issue 
We are having failure on Harmonics of the Camera MCLK and SD card Clock. We have tried with multiple iterations like tuning series resistors of MCLK and SD CLK from 22R to 100R,  reducing drive strength and cable shielding etc but still it does not pass, one observations is when both of them are independently working that time we see that SD is under limit and Camera MCLK goes slighter peak side but issue is when both are running parallel we see major issue.
Till now during all the test iterations we have seen major significant improvements but today (15th APR) we did one test in which seen Good improvement which was done as per below HW modification but still it  is not passing
HW modification we did is in Main board : Inductor value changed to 2.2uH & Placed RC snubber ( R= 2E and C = 680pF) on 3.3V regulator (We see Good Improvement with this rework
 
Here we are attaching 3.3V generation design and 3.3V supply provided  to peripherals. Current drawn on 3.3V is approx 800mA
Also attached RE test results before 3.3V output HW modifications and after 3.3V output HW modification
Please suggest how this HW modifications helped us and what can be done further on supply side if we do have to get still best result and have to pass RE test.