Dear,
We are using BQ76952(5-volt Logic Level) and SPI flash(3.3-volt signal using voltage divider down logic level) on the same SPI bus. But getting the wrong data on Flash register read because if the BQ chip select is HIGH then also BQ holding HIGH MISO pin, that why the Flash MISO pin not providing data. If I reset the BQ (First LOW then High Reset Pin), then only able to get data from Flash but after that not get any response from BQ.
Please help with this. Is there any open drain setting in BQ that can be configured. Please suggest us how can resolve this.