Hi team,
I have made the test setup for LM317 as shown in the image attached here. While testing I have noticed that I'm getting the REF voltage as 1.25V for LM317T/NOPB and for the same setup I'm getting 1.66V for LM317KCT. I would like to know because of what reason this thing is happening. I have given 24V as input and 1.1kOhm and 10kOhm as R1&R2 respectively.