This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256403: output overvoltage because of frequency drop

Part Number: UCC256403


I have designed an LLC resonance converter with a UCC256403 and now I have the following problem.

   ( Key data:
     Uin: 220V < 275V < 320V
     Uout : 24V / 720W
     fnenn: 100kHz )

Unfortunately, the converter only works at higher outputs; at lower output powers, the switching frequency drops depending on the supply voltage.
This also causes the output voltage to rise to unacceptable values.
In the two diagrams I have illustrated this with four different supply voltages.

If I am interpreting the data sheet correctly, the UCC256403 should cover the entire frequency range up to burst mode independently.


Does anyone have any idea which parameter could be responsible for my problem or what I should check?


Thanks in advance !