Hello, I am planning to use LM5165Y (Fixed 3V3 part) in my design for 0.1A load in COT mode. The input voltage to this part goes as low as 3.4V. Considering Equation 4 of section 7.3.4 of datasheet & considering Inductor's DCR of 0.5 ohm DCR & High-Side MOS's RDS of 2 ohm, my understanding is -
When Load is 0.1A, it looks like typical Output voltage will be 3.15V & When Load is 0.02A, it looks like typical Output voltage will be 3.3V can be guaranteed.
Please confirm if my understanding is correct.