Other Parts Discussed in Thread: BQSTUDIO
Hi expert,
Customer uses bq27520-g4 to monitor bat which rated as 3.7V, 3500mAH.
During the test, after several charging/discharging cycles between 0%~100% and 100%~0%, the state of charge stops update stuck at 100% without refreshing.
As below plot, discharge the battery from 4.1V to 3.75V, the state of charge value remains at 100%.
Is it normal? Any suggestions to debug? Thanks!