Hello, I am wondering about the PG output behavior when EN is not active (I am assuming POR and UVLO are OK and EN is used to control the output).
From the datasheet and the related discussion thread, I understand that PG *does not* depend on the state. Is my understanding correct ?
So it would mean that the PG state is not guaranteed while EN is low and PG would depend on the state of OUT over time (through Vds measurement). I am correct ?
Or in other words, if I toogle EN low for a short period of time, then PG state while EN is low would depend on EN low duration and external condition (capacitance on OUT rail and load/no load) ?
Thanks for the clarification.
Pascal