Hi,
(1) For our application (VIN: 12 - 28V, VO: 40 to 80V) we want to implement low-side current sensing (CSP to LED- and CSN to GND) due to the necessity to drive different LED configuations. In the block diagram it can be seen that the TPS92692 uses adaptive slope compensation based on VIN and VCSP. In low-side sensing VSCP will be close to GND. What kind of implications will this have for the slope compensation? Can we still achieve stability with D>0.5? Our max. D will be around 0.8. Could you give us assistance on how to calculate RSLOPE if we use low-side sensing?
(2) To determine closed-loop stability we should only adapt the feedback transfer function (for the changed position of Rcs)? Are there other considerations to achieve closed-loop stabilty?
Thanks in advance.