Other Parts Discussed in Thread: BQ25750
I have a issue with the EVM dev board that having followed the datasheet, EVM user guide and checked voltages on the PCB however I am seeing the error flag "Device in under-voltage protection" Register 24h bit 7
Below is the register dump from Battery Management tool along with screen shots. And help would be great as I must be missing something?
* Created: Tue May 07 14:21:39 BST 2024 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * BQZ Container: Charger_1_00-bq25750.bqz * Charge Voltage Limit 00 10 Charge Current Limit 02 50 Input Current DPM Limit 06 640 Input Voltage DPM Limit 08 348 Reverse Mode Input Current Limit 0A 640 Reverse Mode System Voltage Limit 0C 3E8 Precharge Current Limit 10 14 Termination Current Limit 12 A0 Precharge and Termination Control 14 0B Timer Control 15 0D Three-Stage Charge Control 16 00 Charger Control 17 08 Pin Control 18 C0 Power Path and Reverse Mode Control 19 20 MPPT Control 1A 20 TS Charging Threshold Control 1B 96 TS Charging Region Behavior Control 1C 57 TS Reverse Mode Threshold Control 1D 40 Reverse Undervoltage Control 1E 00 VAC Max Power Point Detected 1F 00 Charger Status 1 21 00 Charger Status 2 22 00 Charger Status 3 23 00 Fault Status 24 80 Charger Flag 1 25 00 Charger Flag 2 26 00 Fault Flag 27 00 Charger Mask 1 28 00 Charger Mask 2 29 00 Fault Mask 2A 00 ADC Control 2B 40 ADC Channel Control 2C 02 IAC ADC - Use Field View 2D 00 IBAT ADC - Use Field View 2F 00 VAC ADC 31 00 VBAT ADC 33 00 VSYS ADC 35 00 TS ADC 37 00 VFB ADC 39 00 Gate Driver Strength Control 3B 00 Gate Driver Dead Time Control 3C 00 Part Information 3D 02 GM Adjust 61 00 Reverse Mode Battery Discharge Current 62 02