This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS652353: Data IN and Enable VLNB out

Part Number: TPS652353

Dear All

Is possible to use the DIN and DOUT (demodulation of external 22KHz tone) when Vlnb out is disable ?

If I set BIT3 in CR2, on pin DIN I have around 2.5V and the 22Khz tone from external source (a receiiver, i.e.)

If I clear BIT3 in CR2, no Vlnb out and on DIN pin voltage drop around 0V , data still present but outside DOUT no data.

If possible with a workaround to use DIN/DOUT decoder also when Vlnb is disable ?

Thanks / Daniele