Hello everyone,
I’m currently testing the LM5019 as a buck converter. The desired output voltage is 15V, and the input voltage range is 18V to 50V. The maximum output current is 60mW.
I used the Excel calculator provided on the component page under Design Tools & Simulation. According to the calculator, it’s recommended to use a Ron resistor of 410kohm, which
yields a nominal switching frequency of about 350KHz. This value is below the maximum allowed frequency at minimum Vin (which is 1MHz).
However, during my testing, I encountered subharmonic oscillation issues at low input voltages (18-20V), the output voltage was 14.46V. There is no mention of subharmonic
oscillation in the datasheet, and I was able to eliminate the issue by raising the switching frequency to 400KHz by reducing the value of Ron.
What could be causing this subharmonic oscillation, and how can I address it?
Thank you for your insights!