Hello ,
I'm utilizing the TPSI3050S to drive a MOSFET in a three-wire configuration. An IR detector is employed for the enable logic, which by default is active, holding the enable pin low. When the light is obstructed, the enable pin receives 4.66V.
On the driver's secondary side, there's a 10V power supply generating , and an RPXFR with a 20Kohm resistor is also in use.
However, the MOSFET's driving pin, VDRV, remains persistently low and does not switch to high.
I need assistance in determining the underlying cause of this issue.
Below is the attached schematic.
For my application, I've chosen an N-channel 200V 130A MOSFET, with the part number IRFP4668PBF from Infineon.