This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: Clarification for connection of VLDOIN pin 5

Part Number: TPSM63606


Hello I have a question regarding connection of TPSM63606 pin 5 (VLDOIN) in a circuit.    Our application has the device configured with Vin = 7.5V, Vout =1.0V providing approx 3A of load current.  Rt = 14.3K = 906Khz.


We have encountered confusion about what to do with the VLDOIN pin:  tie directly to ground or connect 0.1 to 1uF capacitor?  

Currently we have it tied to GND.  Simulation and bench testing show satisfactory operation.  However closer review of the datasheet has caused some confusion.

Table 6-1 of datasheet describes the pin as:  Input bias voltage. Input to the internal LDO that supplies the internal control circuits. Connect to an output voltage point to improve efficiency. Connect an optional high-quality 0.1-μF to 1-μF capacitor from this pin to ground for improved noise immunity. If the output voltage is above 12 V, connect this pin to ground.


Section 8.3-11 of the datasheet provides additional insight about VLDOIN. Here are pertinent snippets from that section:

If the VLDOIN voltage is less than 3.1 V, VIN1 and VIN2 directly power the internal LDO.....

The LDO provides the VCC voltage from one of two inputs: VIN or VLDOIN. When VLDOIN is tied to ground or below 3.1 V, the LDO derives power from VIN. The LDO input becomes VLDOIN when VLDOIN is tied to a voltage above 3.1 V. The VLDOIN voltage must not exceed both VIN and 12 V.

Also in that section graphs 8-5 and 8-6 show Efficiency Increases with External Bias.   The red plots in each are described as "VLDOIN = GND"


Our design is not constrained by efficiency and so we don't need to config the circuit for that metric.  

So our specific questions are:
1) Is our connection of VLDO to GND valid for our configuration?  
2) Are there any negative performance aspects we are unaware of?

Thanks for your review and consideration,

Mark  

  • Hello Mark,

    In your application of VOUT = 1V, I would tie the VLDOIN to GND.

    Given that the output voltage is too low to the VCC voltage derived from the VLDOIN, it is better to tie VLDOIN pin to GND.

    This way on your PCB layout, the VLDOIN pin is connected to GND net and allows another path for heat to dissipate out of the device.

    If you are able to externally provide a 3.3V rail, then the input supply current will be less since in this configuration the internal VCC voltage is not derived from VIN = 7.5V but instead VLDO = 3.3V.

    The benefit of using VLDO is detailed on Figure 8-5 and Figure 8-6 and as you can expect, with higher input voltage the difference in efficiency between VCC powered from VIN versus VCC powered from VLDOIN is more prevalent.

    Hope this helps you with verification of the device.

    Regards,

    Jimmy