Other Parts Discussed in Thread: BQ25792, , TPD6S300, TPS54531, TPS25751, ADS1262, TPS54120
Tool/software:
Hello Sir/Madam
Please help us to check our schematic (attached as pdf), we are using TPS25750 + BQ25792 + TPD6S300 solutions.
I created the schematics based on available documentation and comments from this forum. However, I have a few questions whether everything is done well and whether something can be done better.
The device is to be powered by USB (with 3S battery charging) and enable operation of connected devices in Dual-Role mode (communication with a computer and pendrive/HDD/optional accessories - USB 2.0).
Here are my questions:
1. Is it correct to connect the USB 2.0 differential lines and will it enable communication and PD + BC support ?
2. Can the FLT output of the TPD6S300 be somehow integrated with the TPS25750 ? Do I have to do it myself via the microcontroller in the device ?
3. How to better implement the TPD6S300 power supply ? How is it currently with the 3.3 V LDO in TPS25750, or maybe from the P3V3 power line (TLV75533) ?
4. The forum topic mentioned below mentions possible problems with too large capacitor capacities on the PP5V power line:
Quote from the above-mentioned topic:
The part with the ADC converter will be practically identical to the solution proposed by TI "Design guide: High-Resolution, Low-Drift, Precision Weigh-Scale Reference Design (Rev. A)"
I will be grateful for suggestions on how to best implement the ADC power supply.
Looking forward to your feedback.
Thanks a lot.