This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am having trouble getting the EVM to switch a load above 300mA from the Vin to BATT.
I have seen many post about this on the forum with the fix being updated chipsets.
Have the chipsets been updated? My EVM BQ25750 marking is "TI 3AB AF63 G4".
Hello Alex,
Thanks for working with this.
The default factory settings on the BQ25750 have not been updated and we currently do not plan to update those settings.
To help me with your question, what's the voltage on VIN and BAT when you do the power path switch over?
Best Regards,
Ethan Galloway
Hello Ethan,
My input source is a 4-Series LiFePO4 Pack. ACUV is set to 11Vdc and ACOV is set to 16Vdc.
The BATT input is another 4-Series LiFePO4 Pack. Its BMS is set to operate down to 11Vdc as well.
I am not having any problems charging the battery or switching under 300mA. I believe the problem is the FET drive.
The chipset is trying to turn on the BatFets, but is unable to. I can hear an audible tick when the chipset attempts to turn on the FETs. If i remove the load, then the chipset is able to turn on the FETs.
I encountered a similar problem with the BQ76200 FET driver when using FETs with too high gate capacitance, and too small of a charge pump capacitor.
This is only my theory at this point and I look forward to your feedback.
I have also attached the BQ file from the EVAL module I am using.
* Created: Tue Jun 11 09:00:54 EDT 2024 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * BQZ Container: Charger_1_00-bq25750.bqz * Charge Voltage Limit 00 10 Charge Current Limit 02 640 Input Current DPM Limit 06 640 Input Voltage DPM Limit 08 348 Reverse Mode Input Current Limit 0A 640 Reverse Mode System Voltage Limit 0C 3E8 Precharge Current Limit 10 140 Termination Current Limit 12 A0 Precharge and Termination Control 14 0F Timer Control 15 1D Three-Stage Charge Control 16 00 Charger Control 17 C9 Pin Control 18 C0 Power Path and Reverse Mode Control 19 20 MPPT Control 1A 20 TS Charging Threshold Control 1B 96 TS Charging Region Behavior Control 1C 57 TS Reverse Mode Threshold Control 1D 40 Reverse Undervoltage Control 1E 00 VAC Max Power Point Detected 1F 00 Charger Status 1 21 03 Charger Status 2 22 80 Charger Status 3 23 02 Fault Status 24 00 Charger Flag 1 25 61 Charger Flag 2 26 E0 Fault Flag 27 82 Charger Mask 1 28 00 Charger Mask 2 29 00 Fault Mask 2A 00 ADC Control 2B 60 ADC Channel Control 2C 02 IAC ADC - Use Field View 2D 00 IBAT ADC - Use Field View 2F 00 VAC ADC 31 00 VBAT ADC 33 00 VSYS ADC 35 00 TS ADC 37 00 VFB ADC 39 00 Gate Driver Strength Control 3B 00 Gate Driver Dead Time Control 3C 00 Part Information 3D 02 GM Adjust 61 30 Reverse Mode Battery Discharge Current 62 02
Hello Ethan,
I have confirmed my theory that the BATDRV output was not capable of driving the BATFETs when switching under load.
I took a BQ76200 driver (thats what I had in the lab) and removed R9 from the Eval module. I used the BATDRV to drive the BQ76200's input and put the output directly to the BATFETs.
This method fixed my switching issues, although not elegantly.
What can I do, to make the BQ25750 drive the BATFETs under load without having an external driver?
-Thanks
Hello Alex,
The BQ25750 has built-in over-current protection for the BATFETs. If the discharge current exceeds 8A, the BQ25750 will turn off the BATFETs. There are a few ways to work with this.
The 1st is to use an RC filter to slow down the BATFET turn-on. This will reduce the surge current from BAT to SYS. I also recommend using FETs with a high SOA like the AON6276.
The 2nd is to use the BQ25750's auto reverse mode. Auto Reverse mode will automatically use the converter to provide power to SYS from battery once VAC is removed. The response is really fast and it takes about 50µs for the converter to start working.
Also, I looked through your registers. If you are using the ICHG register to program ICHG, make sure to set WATCHDOG to disabled.
Let me know if you have any questions about this.
Best Regards,
Ethan Galloway
Hello Ethan,
The 8A discharge limit is a problem for my needs. I plan to run the backup battery at 150W so around 13Amps continuous, and I was hoping to use the chipset in stand-alone-mode so I wouldn't have to have it programmed.
I couldn't find the 8Amp limit in the datasheet. Pg.15 states that the max range of the bat sense resistor is ±20Amps, so I assumed that was the max current of the BAT line.
Is there any adjustment for that value or is it a non-changeable setting? Could I change the BAT current sense resistor to possibly get more current?
Hello Alex,
Thanks for being patient with the delay. I was out of office Thursday and Friday.
We are working on adding the 8 amp discharge limit to the datasheet. The max charge current through the converter is still 20A. The discharge current limit through the BATFET can't be changed.
For your application, would it be possible to use auto reverse mode for your application? Auto reverse mode uses the buck-boost converter to send power to the system. The buck-boost converter can handle a 13A discharge.
Best Regards,
Ethan Galloway
Hello Ethan,
Thank you for the information. Unfortunately, my application relies on monitoring the system rail voltage sagging during use, so the reverse mode will not work.
I am a little surprised and disappointed that TI would leave this out of the datasheet, since it extremely important and cannot be changed.
At this point I am working on my own power path control circuit with a separate charge circuit.
Thank you again for your assistance.