Other Parts Discussed in Thread: DRV8220
Tool/software:
Hi,
I'm thinking of using the TPS563257 for a design that needs variable voltage output between 0.6 and 9.5V from 12V input. I'd add resistors in parallel R5 (fig. 8-1 in the datasheet) and make them "switchable" by controlling NPN transistors to GND. Just calculating the resistor values with the equation from 8.2.2.2 of the datasheet gives me the desired results. However, I'd like to know if I may run into more issues, as I can't adapt the inductance (would have to use 4.7µH), and I may trigger protection circuits of the chip if I demand a too-steep voltage change.
I specifically looked for a converter with high switching frequency, so it'll react faster. Ultimately, I'd like to generate a 100Hz sine wave for a load of up to 1A.
thanks!