Tool/software:
Hi team,
Customer input value to understand tstart value is arroung 2[ms]: TPSI305x_calculator_1p24.xlsx
The definition of tstart is the time to VDRV = HIGH from EN=HIGH.

But customer also understands VDDH and VDDM is supplied from VDDP without EN = HIGH. so the charging time to C_DIV should be tstart.
In other words, if C_DIV is charged enough, the time to VDRV= HIGH from EN=HIGH must be t_LH_VDRV (185 us typ) in the datasheet.
Is customer understanding correct? because customer doesn't accept 2ms, require shorter.
So the question is that if Cdiv1 and Cdiv2 charged well after tstart from VDDP supplied, the delay of VDRV and EN must be t_LH_VDRV, is that correct?
Best regards,
Hayashi