This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950-Q1: Automotive qualified Analog controller for PSFB & LLC for 300W standby power supply

Part Number: UCC28950-Q1

Tool/software:

Hi Expert,

Our current project involves the development of a 300W DC-DC power supply. We will  be grateful to get some suggestions from you regarding some potential Analog controllers, that will be best suited for this application.

Topology are also not finalized looking LLC and PSFB, other than this any other suitable topologies are there?

Define the system specifications            
Input parameters Output parameters
Input Power 315.79 W Output power 300 W
Maximum input voltage for Design 450 V Output voltage 15 V
Minimum input voltage for Design 250 V Output current 20.00 A
Nominal Input voltage 400 V Estimated efficiency 95 %



Thank you in advance

Unnimaya.V