This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL5001: Request review a schematic of TL5001.

Part Number: TL5001
Other Parts Discussed in Thread: SN74LVC2G14, SN74LVC3G14, LMG2100R044

Tool/software:

Hi

My customer configured the circuit with TL5001+SN74LVC3G14+SN74LVC2G14+LMG2100R044.

-SPEC-

Input: DC 5V

Output: DC 60V 5A

It didn't work, so we separated TL5001 and LMG2100R044 and carried out the test.
If I give a PWM signal to LGM2100R044, it works well, but if I connect it to TL5001, it doesn't work.
I think the circuit of TL5001 is wrong, could you please review it?

And I'd like to request a review of the schematic, but they don't want to disclose the schematic.
If you tell me how to send it personally, I will send you a schematic.

Thanks