This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460-Q1: SIMPLIS file for part "LM61460-Q1"

Part Number: LM61460-Q1
Other Parts Discussed in Thread: LM61460, SN61460-Q1, LM61440-Q1, LM62440-Q1,

Tool/software:

Can you share the SIMPLIS file for part "LM61460(SN61460)?

------------------------------------------------------------------------------------------------------------------

SN61460 : SN61460-Q1 3-V to 36-V, 6-A, Low EMI Synchronous Step-Down Converter

Suitable for scalable power supplies

 – Pin compatible with:

     • LM61440-Q1 (36 V, 4 A, adjustable fSW)

     • LM62440-Q1 (36 V, 4 A, fixed fSW)

     • LM61460-Q1 (36 V, 3 A, adjustable fSW)

-------------------------------------------------------------------------------------------------------------------