UCC27531-Q1: 2-switch flyback topology. UCC27531-Q1 to drive SiC mosfet

Part Number: UCC27531-Q1
Other Parts Discussed in Thread: UCC27624, UCC27531

Tool/software:

I am planning to use the UCC27531-Q1 2.5-A and 5-A, 35V MAX VDD FET and IGBT Single-Gate Driver to drive the SCT2H12NZ 1700V, 3.7A, THD, Silicon-Carbide (SiC) MOSFET in a 2-switch flyback topology. An example of my schematic is attached. Could you please help me understand if there might be any issues with this setup?



SCT2H12NZ Mosfet Information,