TPS1H200A-Q1: TPS1H200A-Q1

Part Number: TPS1H200A-Q1

Tool/software:

Hi,

I am thinking about using the high-side switch to control a solenoid. 

I am in a power sensitive application, so I am looking for a Peak and hold solution.

On the solenoid datasheet data is like this:

Coil Resistance 289 ohm

Pull-In @ 20 dg C 7V, 18 mA @0 bar

Drop-Out @ 20 dg C 3V, 3.5 mA @6 bar

Power Rating 0.5W

The solenoid have diodes included(flyback)

The datasheet of TPS1H200A-Q1, show that the flyback diode should be place differently from directly on the solenoid.

So what do you suggest?

Extra info I need a solution for 8 valves and open to other suggestions.