Tool/software:
Hi,
The calculation method provided in the article cannot be accessed. Do you have an alternative calculation method?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
The calculation method provided in the article cannot be accessed. Do you have an alternative calculation method?
Hi,
For output inductor, its inductance design can be seen on n this application note.
https://www.ti.com/lit/an/slua535a/slua535a.pdf?ts=1720257390204
But if you want to design an inductor that is completely different from design an inductor value. You can search the internet to find how to design an inductor after you know the inductor specs based on the above application note.
HI,
After reviewing the documentation, I noticed that section 4.1.1 only mentions the inductance value but does not mention the calculation of the turns ratio.
I would like to know why the output inductor turns ratio used in the LM5025AEVAL is 4:13.
Thank you for your reply.
Hi,
B0358 specs show pri:sec = (1-2):(3:4) = 13:4 = 3.25:1, this is to help make auxiliary bias power to LM5025A VCC.
When L2 current is in freewheeling, L2 (4 to 3) is connected to Vout = 3.3V which making L2 (2 to 1) is 3.3V x 3.25 = 10.7V, which is required between 8V and 15V for VCC based on the datasheet recommendation.