This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260-Q1: Output 52V under EFT test

Part Number: TPS54260-Q1

Tool/software:

Hi Expert,

My customer found the output of TPS54260-Q1 is 52V, not 0V, under the EFT test. Though he try add some Caps or TVS, but these methods doesn't work. 

The schematic, test input waveform and output waveform as below figures. And the switch frequency is 350KHz, the input EFT frequency is > 350kHz.

Can you help analysis the issue and give some advice?