Tool/software:
I have a problem when using the wireless charger. This is my setup:
-
TX coil is a Baseus QI charger. It has an LED indicator which is very handy for resolving issues.
-
RX coil is a TDK WR222230-26M8-G 27uH and 22 mm diameter.
-
BQ51013B configured for wireless charger and USB charger. Both EN1 and EN2 are pulled down to make USB charger the default source. An LED is connected to /CHG to provide a visual representation when the device is charging.
-
A BQ25120AYFPR battery charger.
The schematic is as follows:


I see the following behavior:
-
When I only use the USB charger, Vout is 5V as expected, but the D1 LED doesn't turn on, so I assume /CHG is not pulling down but /AD-EN is.
-
When I only use the wireless charger, Vout is 0V, and the D1 LED doesn't turn on.
-
When I plug both power sources, the output depends on the EN2 value as expected: 0V when pulled up, 5V when pulled down. D1 LED doesn't turn on.
I am fairly confident that the BQ51013B is communicating correctly with the Baseus charger. I have performed the following tests:
-
At first, I placed the wrong resonant capacitor, and the Baseus charger didn't react to the RX coil. The Baseus LED indicator was constantly on.
-
When I placed the correct capacitor, the Baseus LED was blinking slowly, which means it is charging. With the oscilloscope, I can see that Vrec is approximately 7.4V, and the power consumption of the Baseus charger is approximately 1W. When I separate a few mm from the RX coil from the TX coil, I can see that Vrec voltage drops briefly but is adjusted again to 7.4V, and the charger consumption increases to 4W. I assume this means that the RX coil is correctly communicating with the TX coil to increase power output.
-
If I force a failure by removing the 10K NTC, the Baseus charger LED flashes rapidly to indicate failure, and I can only see a ping that lasts a few ms on my oscilloscope. This to me confirms that there is actually communication between the two coils.
-
If I connect the Baseus charger and the USB power at the same time, the Baseus LED stays ON (not charging), and I can only see a ping on my oscilloscope.
I don't know what's causing the BQ51013B to not output any voltage on Vout. I have tried replacing the BQ51013B, but that didn't solve the issue.
Thank you in advance.