This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28742: AC - DC Power Supply part selection

Part Number: UCC28742UCC256402
Other Parts Discussed in Thread: UCC28950, UCC28251, UCC2894, UCC256402, UCC25640EVM-020, UCC25640

Tool/software:

Hi,

I am designing a Power supply having following parameters:

  • Input Voltage: 85VAC - 265VAC
  • Input Frequency: 50Hz - 60Hz
  • Output Voltage: 12V DC
  • Output Current: 25A
  • Protection: input under-voltage protection, input over-voltage protection, input surge protection, output over-voltage protection, output over-current protection

Need to find a suitable part for it.