Other Parts Discussed in Thread: TPS709
Tool/software:
For the output voltage accuracy, there seems two parts.
One is the internal reference, and the other part is output voltage accuracy.
The customer is calculating the maximum output voltage.
So whether they should considering 1.24V + 4% error? Which means when the output voltage is 15V, the maximum could be 15*(1.24/1.205)*(1+4%)=16.05V.
Is it right?
The voltage accuracy is not so good. The customer is worried about this.
Could you explain how we get the output voltage accuracy -4%~+4% and get rid of the customer's concern.