Tool/software:
Hi TI Expert,
I would like to clarify the definition of the ΔVOUT marked in the TPS7A21-Q1 datasheet.
In first row, assume the VOUT is 4V, the VOUT range will be (4V*97.75%) ~ (4V *101.5%)?
That will be 3.91V~4.06V, am I right?
In the forth row, assume VOUT is 2V, the VOUT range will be 1.93V ~ 2.05V?
For the Line regulation:
Assume VOUT= 3V, ΔVin = 1V (5V VIN -> 4V VIN), the IOUT = 1mA.
The ΔVOUT will be 0.03% * 1V * 3V = 0.9mV, so VOUT will be (3V + 0.9mV) or (3V - 0.9mV)?
For the load regulation,
Assume VOUT = 3V, ΔIOUT = 200mA(from 1mA -> 201mA), I believe the VOUT will be 3V - (3V * 0.003% * 200) = 2.982V?
Please correct me if I was wrong.
Thank you.