This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616EVM-021: i have received no reply from the board via uart, communicating directly from the mcu with bq79616

Part Number: BQ79616EVM-021
Other Parts Discussed in Thread: BQ79616, TMS320F280039C, USB2ANY

Tool/software:

I'm trying to communicate with the BQ79616 board with the TMS320F280039C MCU directly via UART, I'm using a baud rate of 1Mbsp, I send the wakeup the led turns on then I try to make a reading and I get no response on the TX.

I only have J2 shunted, I would like to know if there is any configuration that needs to be done to be able to communicate with the board.

Thank you