Tool/software:
Hi
I have a battery pack, After charging is completed, FFC is updated to 0;
After the abnormality, the FCC is also updated to 0 after the discharge is completed.
Please help analyze the cause of the problem.0.2C discharge-FCC update 0.log
Thu Jul 11 09:07:46 CST 2024 Device Version Info = 1746_0_01 BQZ Device Name = bq27z746 BQZ Firmware Version = 0_01 Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,MaxLoadCurrent,MaxLoadTimeEmty,VoltHiSet,VoltHiClear,VoltLoSet,VoltLoClear,TempHiSet,TempHiClear,TempLoSet,TempLoClear,SOCDeltaSet,BTPDsgSet,BTPChgSet,IntStatus,ChgCurr,ChgVolt,QmaxCC,TermV,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,BattSenseOutput,BattSenseStatus,SafetyAlert 1,SafetyAlert 2,SafetyStat 1,SafetyStat 2,Elapsed Time,PackPinV,CellVolt,CellCurr,CellPower,IntTemp,TS1Temp,TS1Temp,CellTemp,FETTemp,Cell1RawV,CellRawI,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,CompRes1,PackGrid,LStatus,CellGrid1,StateTime,DOD0_1,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,QMax1,QMaxDOD0_1,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2024-07-11 09:07:51,4.014,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104002,3337,3337,0,0,24.5,24.3,-273.2,24.3,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55578,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1016,SUCCESS 2,2024-07-11 09:07:55,8.017,0x0054,-4606,22,24.1,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104006,3338,3337,0,0,24.7,24.1,-273.2,24.1,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.1,1000,0,13,14,0,55582,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,997,SUCCESS 3,2024-07-11 09:07:59,12.030,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104010,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,0,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55586,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1031,SUCCESS 4,2024-07-11 09:08:03,16.032,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104014,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-4,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55590,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,995,SUCCESS 5,2024-07-11 09:08:07,20.033,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0440,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104018,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55594,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,995,SUCCESS 6,2024-07-11 09:08:11,24.051,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104022,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55598,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,994,SUCCESS 7,2024-07-11 09:08:15,28.031,0x0054,-4606,22,24.0,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104026,3338,3337,0,0,24.6,24.0,-273.2,24.0,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.0,1000,0,13,14,0,55602,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1012,SUCCESS 8,2024-07-11 09:08:19,32.030,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104029,3339,3337,0,0,24.6,24.3,-273.2,24.3,-273.2,3337,-4,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55606,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,998,SUCCESS 9,2024-07-11 09:08:23,36.030,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104033,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55610,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1001,SUCCESS 10,2024-07-11 09:08:27,40.052,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0440,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104038,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55614,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,990,SUCCESS 11,2024-07-11 09:08:31,44.055,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104042,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55618,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,989,SUCCESS 12,2024-07-11 09:08:35,48.057,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104046,3340,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,0,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55622,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1004,SUCCESS 13,2024-07-11 09:08:39,52.057,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104050,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55626,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1051,SUCCESS 14,2024-07-11 09:08:43,56.058,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104054,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,0,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55630,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1003,SUCCESS 15,2024-07-11 09:08:47,60.052,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0440,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104057,3338,3337,0,0,24.6,24.3,-273.2,24.3,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55634,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1008,SUCCESS 16,2024-07-11 09:08:51,64.052,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104061,3338,3337,0,0,24.6,24.3,-273.2,24.3,-273.2,3337,-2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55638,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,980,SUCCESS 17,2024-07-11 09:08:55,68.052,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104065,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,0,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55642,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,976,SUCCESS 18,2024-07-11 09:08:59,72.047,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104069,3337,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,-4,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55646,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,997,SUCCESS 19,2024-07-11 09:09:03,76.050,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104073,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55650,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1025,SUCCESS 20,2024-07-11 09:09:07,80.067,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0440,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104077,3337,3337,0,0,24.6,24.3,-273.2,24.3,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55654,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1025,SUCCESS 21,2024-07-11 09:09:11,84.066,0x0054,-4606,22,24.3,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104081,3337,3337,0,0,24.6,24.3,-273.2,24.3,-273.2,3337,2,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.3,1000,0,13,14,0,55658,878,0,0,7,0,1886,0,0,245,9.91,10042,1152,0,0,1013,SUCCESS 22,2024-07-11 09:09:15,88.069,0x0054,-4606,22,24.2,3337,0,0,0,95,1671,1772,65535,65535,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x8386,0x0040,0x08,0x0084,0x40,0x2D11,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104085,3338,3337,0,0,24.6,24.2,-273.2,24.2,-273.2,3337,0,1671,531,1772,564,1671,531,101,33,1772,564,24.2,24.2,1000,0,13,14,0,55662,878,0,0,7,0,1886,0,0,245,9.91,10042,1184,0,0,1004,SUCCESS 23,2024-07-11 09:09:19,92.065,0x0054,-4606,22,24.2,3372,898,898,303,95,1671,1772,65535,15,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0004,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104089,3380,3372,898,303,24.6,24.5,-273.2,24.5,-273.2,3381,898,1672,530,1772,563,1665,530,102,33,1767,563,24.2,24.2,1000,0,13,14,0,1,890,0,0,0,0,1886,890,0,0,9.91,10042,1184,0,0,1041,SUCCESS 24,2024-07-11 09:09:23,96.065,0x0054,-4606,22,24.3,3405,900,899,304,95,1672,1772,65535,15,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104093,3416,3405,898,306,24.6,24.3,-273.2,24.3,-273.2,3415,900,1673,530,1772,563,1666,530,102,33,1767,563,24.2,24.2,1000,0,13,14,0,5,890,-1,0,0,0,1886,890,-1,0,9.91,10042,1184,0,0,1059,SUCCESS 25,2024-07-11 09:09:27,100.064,0x0054,-4606,22,24.3,3443,900,899,305,95,1673,1772,65535,15,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104097,3454,3443,898,309,24.5,24.2,-273.2,24.2,-273.2,3454,900,1674,530,1772,563,1667,530,102,33,1767,563,24.2,24.2,1000,0,13,14,0,9,890,-2,0,0,0,1886,890,-2,0,9.91,10042,1184,0,0,1042,SUCCESS 26,2024-07-11 09:09:31,104.064,0x0054,-4606,22,24.3,3488,898,899,307,95,1674,1772,65535,15,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104101,3497,3488,900,314,24.5,24.3,-273.2,24.3,-273.2,3502,900,1675,530,1772,563,1668,530,102,33,1767,563,24.2,24.2,1000,0,13,14,0,13,890,-3,0,0,0,1886,890,-3,0,9.91,10042,1184,0,0,1011,SUCCESS 27,2024-07-11 09:09:35,108.063,0x0054,-4606,22,24.3,3525,645,862,296,95,1675,1772,65535,15,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104105,3534,3525,669,236,24.5,24.3,-273.2,24.3,-273.2,3532,605,1675,531,1772,563,1669,531,102,33,1767,563,24.2,24.2,1000,0,13,14,0,17,890,-4,-1,0,0,1886,890,-4,0,9.91,10042,1184,0,0,1027,SUCCESS 28,2024-07-11 09:09:39,112.094,0x0054,-4606,22,24.3,3546,453,778,268,95,1676,1772,65535,17,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104109,3552,3546,466,165,24.6,24.3,-273.2,24.3,-273.2,3550,424,1676,531,1772,563,1670,531,102,33,1767,563,24.2,24.2,1000,0,13,14,0,21,890,-5,-1,0,0,1886,890,-5,0,9.91,10042,1184,0,0,1091,SUCCESS 29,2024-07-11 09:09:43,116.095,0x0054,-4606,22,24.3,3558,335,680,235,95,1676,1772,65535,18,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104113,3563,3558,341,121,24.5,24.2,-273.2,24.2,-273.2,3561,323,1676,531,1772,563,1670,531,102,33,1767,563,24.2,24.2,1000,0,13,14,0,25,890,-5,-1,0,0,1886,890,-5,0,9.91,10042,1184,0,0,1056,SUCCESS 30,2024-07-11 09:09:47,120.093,0x0054,-4606,22,24.2,3567,256,584,203,95,1676,1772,65535,20,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104117,3571,3567,264,94,24.5,24.2,-273.2,24.2,-273.2,3568,245,1677,531,1772,563,1670,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,29,890,-5,-1,0,0,1886,890,-5,0,9.91,10042,1184,0,0,1060,SUCCESS 31,2024-07-11 09:09:51,124.093,0x0054,-4606,22,24.2,3572,205,497,173,95,1677,1772,65535,22,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104121,3575,3572,206,74,24.5,24.2,-273.2,24.2,-273.2,3573,203,1677,531,1772,563,1670,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,33,890,-5,-1,0,0,1886,890,-5,0,9.91,10042,1184,0,0,1090,SUCCESS 32,2024-07-11 09:09:55,128.080,0x0054,-4606,22,24.2,3576,170,421,147,95,1677,1772,65535,24,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104125,3579,3576,171,61,24.5,24.2,-273.2,24.2,-273.2,3576,160,1677,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,37,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1043,SUCCESS 33,2024-07-11 09:09:59,132.094,0x0054,-4606,22,24.3,3579,142,356,125,95,1677,1772,65535,26,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104129,3581,3579,142,51,24.5,24.2,-273.2,24.2,-273.2,3579,136,1677,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,41,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1044,SUCCESS 34,2024-07-11 09:10:03,136.080,0x0054,-4606,22,24.3,3581,120,301,106,95,1677,1772,65535,31,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104133,3583,3581,120,43,24.5,24.2,-273.2,24.2,-273.2,3581,120,1677,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,45,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1011,SUCCESS 35,2024-07-11 09:10:07,140.093,0x0054,-4606,22,24.3,3583,105,255,90,95,1677,1772,65535,34,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104137,3584,3583,105,38,24.5,24.3,-273.2,24.3,-273.2,3583,98,1677,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,49,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1062,SUCCESS 36,2024-07-11 09:10:11,144.096,0x0054,-4606,22,24.3,3584,92,217,76,95,1677,1772,65535,40,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104141,3586,3584,92,33,24.5,24.3,-273.2,24.3,-273.2,3584,88,1677,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,53,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1041,SUCCESS 37,2024-07-11 09:10:15,148.099,0x0054,-4606,22,24.3,3585,79,185,65,95,1678,1772,65535,47,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104145,3587,3585,79,28,24.5,24.3,-273.2,24.3,-273.2,3585,77,1678,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,57,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1057,SUCCESS 38,2024-07-11 09:10:19,152.097,0x0054,-4606,22,24.3,3586,72,159,56,95,1678,1772,65535,43,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104149,3588,3586,72,26,24.5,24.2,-273.2,24.2,-273.2,3586,70,1678,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,61,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1058,SUCCESS 39,2024-07-11 09:10:23,156.097,0x0054,-4606,22,24.3,3586,66,137,48,95,1678,1772,65535,47,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104153,3588,3586,66,24,24.6,24.2,-273.2,24.3,-273.2,3587,61,1678,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,65,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1056,SUCCESS 40,2024-07-11 09:10:27,160.094,0x0054,-4606,22,24.3,3587,59,119,42,95,1678,1772,65535,52,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104157,3588,3587,57,20,24.6,24.3,-273.2,24.3,-273.2,3588,55,1678,531,1772,563,1671,531,102,33,1767,563,24.2,24.1,1000,0,13,14,0,69,890,-6,-1,0,0,1886,890,-6,0,9.91,10042,1184,0,0,1058,SUCCESS 41,2024-07-11 09:10:31,164.095,0x0054,-4606,22,24.3,3588,53,104,37,95,1678,1772,65535,57,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104161,3589,3588,53,19,24.6,24.3,-273.2,24.3,-273.2,3588,50,1678,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,73,890,-7,-2,0,0,1886,890,-7,0,9.91,10042,1184,0,0,1061,SUCCESS 42,2024-07-11 09:10:35,168.095,0x0054,-4606,22,24.3,3588,50,91,32,95,1678,1772,65535,63,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0008,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104165,3589,3588,48,17,24.6,24.2,-273.2,24.2,-273.2,3588,48,1678,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,77,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1061,SUCCESS 43,2024-07-11 09:10:39,172.094,0x0054,-4606,22,24.3,3588,48,81,29,95,1678,1772,65535,70,-702,143,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104169,3590,3588,46,17,24.6,24.3,-273.2,24.3,-273.2,3589,48,1678,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,81,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1077,SUCCESS 44,2024-07-11 09:10:43,176.112,0x0054,-4606,22,24.3,3589,42,72,25,96,1685,1772,65535,79,-702,144,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104173,3591,3589,41,15,24.6,24.3,-273.2,24.3,-273.2,3589,39,1687,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,85,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1059,SUCCESS 45,2024-07-11 09:10:47,180.111,0x0054,-4606,22,24.3,3589,39,64,23,96,1694,1772,65535,89,-702,145,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104177,3590,3589,41,15,24.6,24.3,-273.2,24.3,-273.2,3589,37,1697,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,89,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1058,SUCCESS 46,2024-07-11 09:10:51,184.112,0x0054,-4606,22,24.3,3590,37,58,21,97,1704,1772,65535,98,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104181,3591,3590,39,14,24.6,24.3,-273.2,24.3,-273.2,3590,37,1706,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,93,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1073,SUCCESS 47,2024-07-11 09:10:55,188.113,0x0054,-4606,22,24.3,3584,0,44,16,97,1709,1772,65535,130,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104185,3585,3584,0,0,24.6,24.3,-273.2,24.3,-273.2,3583,0,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,97,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1039,SUCCESS 48,2024-07-11 09:10:59,192.110,0x0054,-4606,22,24.3,3581,0,34,12,97,1709,1772,65535,168,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104189,3582,3581,0,0,24.5,24.3,-273.2,24.3,-273.2,3580,4,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,101,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1029,SUCCESS 49,2024-07-11 09:11:03,196.112,0x0054,-4606,22,24.3,3577,0,26,9,97,1709,1772,65535,219,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104193,3579,3577,0,0,24.6,24.3,-273.2,24.3,-273.2,3576,-2,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,105,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1041,SUCCESS 50,2024-07-11 09:11:07,200.110,0x0054,-4606,22,24.3,3574,0,19,7,97,1709,1772,65535,300,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104197,3575,3574,0,0,24.6,24.3,-273.2,24.3,-273.2,3573,-2,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,109,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1044,SUCCESS 51,2024-07-11 09:11:11,204.127,0x0054,-4606,22,24.3,3572,0,15,5,97,1709,1772,65535,380,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104201,3573,3572,0,0,24.6,24.2,-273.2,24.3,-273.2,3571,0,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,113,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1030,SUCCESS 52,2024-07-11 09:11:15,208.126,0x0054,-4606,22,24.3,3569,0,11,4,97,1709,1772,65535,518,-702,146,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x0080,7,100,0x0386,0x0040,0x08,0x0808,0x00,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104205,3570,3569,0,0,24.6,24.2,-273.2,24.3,-273.2,3569,-2,1709,532,1772,563,1672,532,102,33,1767,563,24.2,24.1,1000,0,13,14,0,117,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1030,SUCCESS 53,2024-07-11 09:11:19,212.487,0x0054,-4606,23,24.3,3567,0,9,3,100,1769,1769,65535,633,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104210,3570,3565,0,0,24.6,24.3,-273.2,24.6,-273.2,3566,2,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,121,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1010,SUCCESS 54,2024-07-11 09:11:23,216.126,0x0054,-4606,23,24.3,3565,0,6,2,100,1769,1769,65535,950,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,0,0,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104213,3109,3565,0,0,24.7,24.3,-273.2,24.3,-273.2,3565,-2,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,125,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,1029,SUCCESS 55,2024-07-11 09:11:27,220.142,0x0054,-4606,23,24.3,3563,0,5,2,100,1769,1769,65535,1140,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,0,0,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104217,3107,3563,0,0,24.6,24.3,-273.2,24.3,-273.2,3563,0,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,129,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,998,SUCCESS 56,2024-07-11 09:11:31,224.127,0x0054,-4606,23,24.3,3562,0,4,1,100,1769,1769,65535,1425,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,0,0,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104221,3105,3562,0,0,24.6,24.3,-273.2,24.3,-273.2,3561,2,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,133,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,997,SUCCESS 57,2024-07-11 09:11:35,228.126,0x0054,-4606,23,24.3,3560,0,3,1,100,1769,1769,65535,1900,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,0,0,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104225,3104,3560,0,0,24.6,24.3,-273.2,24.3,-273.2,3560,-2,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,137,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,998,SUCCESS 58,2024-07-11 09:11:39,232.126,0x0054,-4606,23,24.3,3559,0,2,1,100,1769,1769,65535,2850,-702,151,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,0,0,7,32767,0x40A0,7,100,0x4382,0x0040,0x08,0x0088,0x0A,0x2D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104229,3102,3559,0,0,24.6,24.3,-273.2,24.3,-273.2,3558,0,1769,564,1769,564,1769,564,102,33,1769,564,24.3,24.1,1000,0,13,14,0,141,890,-7,-2,1,0,1886,890,-7,1,9.91,10042,1184,0,0,981,SUCCESS 59,2024-07-11 09:11:43,236.130,0x0054,-4606,21,24.3,3479,-901,-377,-134,90,1592,1769,253,65535,-901,106,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x00C0,7,100,0x0386,0x0040,0x08,0x0008,0x60,0x3D18,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,16104234,3447,3453,-900,-311,24.6,24.3,-273.2,24.3,-273.2,3433,-900,-1,0,92,30,-1,0,92,30,92,30,24.3,24.1,1000,0,1,14,1,3,798,1,0,0,0,1886,890,-6,1,9.91,10042,0,0,0,1135,SUCCESS 60,2024-07-11 09:11:47,240.143,0x0054,-4606,0,24.4,3398,-901,-503,-176,0,0,92,0,65535,-901,0,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x08D0,7,100,0x0386,0x0040,0x08,0x0004,0x65,0x3D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104237,3391,3398,-900,-306,24.6,24.4,-273.2,24.4,-273.2,3384,-900,-2,0,92,30,-2,0,92,30,92,30,24.3,24.1,1000,0,1,14,1,7,798,2,0,0,0,1886,890,-5,1,9.91,10042,0,0,0,981,SUCCESS 61,2024-07-11 09:11:51,244.141,0x0054,-4606,0,24.4,3354,-900,-598,-206,0,0,92,0,65535,-901,0,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x08D0,7,100,0x0386,0x0040,0x08,0x0004,0x65,0x3D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104241,3346,3354,-900,-302,24.7,24.4,-273.2,24.4,-273.2,3346,-900,-3,-1,92,30,-3,-1,92,30,92,30,24.3,24.1,1000,0,1,14,1,11,798,3,1,0,0,1886,890,-4,1,9.91,10042,0,0,0,1030,SUCCESS 62,2024-07-11 09:11:55,248.143,0x0054,-4606,0,24.4,3325,-900,-671,-229,0,0,92,0,65535,-901,0,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x08D0,7,100,0x0386,0x0040,0x08,0x0004,0x65,0x3D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104245,3316,3325,-900,-299,24.7,24.4,-273.2,24.4,-273.2,3319,-905,-3,-1,92,30,-4,-4,92,30,92,30,24.3,24.1,1000,0,1,14,1,15,798,4,4,0,0,1886,890,-3,1,9.91,10042,0,0,0,1027,SUCCESS 63,2024-07-11 09:11:59,252.142,0x0054,-4606,0,24.5,3304,-900,-726,-245,0,0,92,0,65535,-901,0,5000,0,18,574,-18,0,0,-3,35,-1,-1,0x14,900,3600,7,32767,0x08D0,7,100,0x0386,0x0040,0x08,0x0004,0x65,0x3D18,0x0038,0x60,0x00,0x0000,0x0000,0x0000,0x0000,16104249,3296,3304,-901,-298,24.7,24.5,-273.2,24.5,-273.2,3300,-901,-4,-4,92,30,-5,-7,92,30,92,30,24.3,24.1,1000,0,1,14,1,19,798,5,7,0,0,1886,890,-2,1,9.91,10042,0,0,0,1028,SUCCESS