This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25306: Can the STAT pin be directly connected to a MCU GPIO with an internal pull-up?

Part Number: BQ25306


Tool/software:

I am not finding an explicit confirmation in the bq25306 datasheet that the STAT pin can be connected to a MCU GPIO with an internal pull-up.  The reason I ask is that we are seeing the STAT pin glitch several times over a period of about one second when VBUS is connected and when the battery reaches a charged state.   Are there any requirements for the STAT pin pull-up voltage or pull-up resistor value?

Thank you.