Other Parts Discussed in Thread: BQ25756
Tool/software:
Hi everyone,
for a customer application I want to use the BQ25750. In this project I'll must to request an input current of 20A max and a input voltage that change from 5V to 60V . I'll wish to know up to how many mosfet in I can put in parallel, and which is the massimun output current of embedded driver.
For the H-bridge I want to use the BSC035N10NS5ATMA1 MOSFET, that have Qg max = 87nC.
Eventually, is it possible to use an external high/low side driver? And if it's yes, how I can connect it to BQ25750?
Thank you for your attention
Paolo A.