Other Parts Discussed in Thread: TPS92692
Tool/software:
Hi Team,
My customer is evaluating TPS92692-Q1 in their project, could you please help give some comments for below questions?
When the customer is using the TPS92692 as a BOOST topology architecture, there are some issues with the PMOS selection on the output side, as shown in Q1 in the following figure.
The customer would like to know how long does the voltage of the CSP-CSN trigger the OCP to the PDRV shutdown PMOS during the output short circuit to ground? The purpose of this question is that customers in selecting this PMOS, PMOS needs to withstand this short circuit current in the time between output short circuit to IC off,
The current design requirement is an output current of 200mA and an output voltage of 35V.
Thanks,
Regards,
Ivy