This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2842: How to determine the value of the input capacitance of the flyback power supply?

Part Number: UC2842
Other Parts Discussed in Thread: UC3842

Tool/software:

Dear experts,

      The flyback power supply input voltage is 24VDC ,Vout=16V  and the input capacitor is 9 x 10uF MLCCs in parallel.

      When the flyback power supply is loaded with 1A, the input voltage fluctuates violently PP-1.35V, and the yellow waveform is the input voltage ripple.

      Why does the input voltage fluctuate with the increase of load, and how to calculate the value of the input capacitance with DC input.I find a calculation method in UC3842's datasheet but it calculate with a rectifier bridge

   Thankyou