TPS25750: How to limit the value of the input voltage

Part Number: TPS25750
Other Parts Discussed in Thread: TPS25751

Tool/software:

We use TPS25750 for evaluation.

We wants to use TPS25750 for sink device(special specification charger).
This charger only allow 5V/1A and 20V/2A.

If we try to set 5V/1A and 20V/2A to Sink capability (Reg: 0x33).
But TPS25750 request 9V/2.22A to source.(AC adaptor(source) capability is 5V/3A, 9V/2.22A, 12V/1.5A)
Our expect is 5V/3A in this case.

Could you tell me how can we limit a input voltage in sink function?

___________________________                                                      __________________________________
|                                                     |                                                     |                                                                   |
|            AC Adaptor(USB PD)       |                                                     | Special Charger with TPS25750               |
|     5V/3A, 9V/2.22A, 12V/1.5A     |=========================|                 5V/1A, 20V/2A                           |
|                    Source                      |                 USB Type-C               |                       Sink                                      |
---------------------------------------------                                                      ---------------------------------------------------------
                                                                 9V/2.22A negothiated.