Other Parts Discussed in Thread: TPS54320, TPSM82914, TPS62914, LM2641, TPS543620
Tool/software:
Can you suggest a similar BUCK converter for the 4A output current?
My input voltage is 12V+-10%, and output voltage is 3.3V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Harsh,
If you're looking to stay in the same family where the footprint would be the same, you can use TPS54320 (3A) however it's a bit below your need.
On the other hand, we have buck converters with 4A with same Current Mode mechanism which include converter: TPS62914 or it's module: TPSM82914. At 5A max we have LM2641 also with Current Mode. Lastly, if you are looking for a newer device, we have TPS543620 (6A) which incorporates Advanced Current Mode.
Regards,
Eileen