Tool/software:
Ti's experts:
We use the BQ27742-G1 chip, and the schematic diagram is shown below. When testing the ESD of the whole machine by the end customer, there is a communication abnormality. May I ask what is the maximum resistance that can be used for these resistors?
At present, testing has found that there is no problem with 510 Ω. Can it be used?
We used a series connection of 2 100 Ω resistors and added ESD diodes
Look forward to your reply
Thanks