Other Parts Discussed in Thread: UCC14241-Q1,
Tool/software:
Hi,
We have a UCC14240 connected to a UCC5870 Gate Driver as part of an inverter design. The output from the UCC14240 is 0.0V on all outputs, the device uses about 1mA at 24V.
Our required output is +20V, -5V. As such we have followed the UCC1424x design spreadsheet and have both FBVEE resistors at 49.9K, FBVCC resistors at 10K and 69.8K. ILim is 270R.
VEE-COM Capacitors are about 40uF, COM-VCC Capacitors are about 22uF.
Our VIn is +24VDC, the ENA pin is at 4.1V and the PG pin has a 10K pullup to 3.3V
Our schematic is below.
Our board layout showing the key compoennts:
Can anyone suggest what to check to determine why we are getting no output? We are totally lost as to why the devices have 0V output.
Thanks