This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: LODRV MOSFET blowing on battery plugin

Part Number: BQ24610

Tool/software:

I am trying to design a battery charger that fits within a larger system. It uses two 11.1V Li Ion battery packs connected in series to create a nominal 22.2V battery.

See schematic here: battery-charger-24v.pdf

When I connect the batteries, the board gets damaged in some way that means that power BATT and GND become shorted together. Using a thermal imaging camera shows the LODRIV mosfet getting very hot, although I can't be sure that this part is the one that gets damaged or if it is the IC itself. Doing some basic probing it does seem like the MOSFET gets damaged. I had this issue and then replaced the MOSFET with one rated much higher (100V) and it is still giving issues.

Other notes about the design:

  •  We are not worried about limiting the AC adapter current
  • We are aiming for battery longevity so the charge current is set to 0.5A and the charge voltage to 23.5V
  • The batteries have their own battery protection IC so there is no thermistor.
  • The BATT output is connected to a diode on another board (but the board gets damaged before being attached to the other board, so I think unlikely to be the source of the problem)