This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS27081A: TPS27081A

Part Number: TPS27081A
Other Parts Discussed in Thread: TPS22975

Tool/software:

Hi, 

I am searching  for a load switch with higher current ( 5A ) with this package (SOT-23-6 Thin, TSOT-23-6), if is anything is available Please let me know. 

Note:- We are using this part no (TPS27081ADDCR), this is with 3A. Now we need to change with 5A with same pin mapping. 

Thanks, 

Jahanvi

  • Hi Jahanvi,

    We don't have similar devices (6 pin or SOIC/SOT package with 5A current carrying capacity). Also most of our load switches are NFET based. This one is PFET based. 

    For 5A load switches, I can recommend devices like TPS22975 which is 6A device with smaller package size (4mm^2).

    Best Regards,
    Arush