Hello,
I have a customer who would like to operate the LM5005 with a clock frequency higher than 500kHz; however, the datasheet is not 100% clear on this. According to the first page and the RT pin description, the recommended range is 50kHz to 500kHz. However, there is a graph on page 6 of the datasheet that shows an operating range up to 800kHz with a RT=5K. Can the LM5005 operate safely above 550kHz up to 800kHz? My customer would like to set this frequency between 625kHz and 650kHz..
Thanks,
Ali