WE ARE HAVING DIFFCULTY MEETING THE 3% HARMONIC & 5% MAX THD LEVELS ON THE 3RD & 5TH HARMONICS USING THE UCC28051 PFC CONTROLLER ON A 35W CV SWITCHING SUPPLY
WE MUST MEET THIS SPEC DOWN TO A 10W LOAD LEVEL FOR A MILITARY PROJECT. OUR 3RD HARMONIC MEASURES ABOUT 4.67% AT A 20W LEVEL. THE MAIN PWM IS RUNNING AT 65KHZ. WILL VARYING THE SWITCHING FREQ LOWER THE HARMONICS?
I UNDERSTAND THAT THE EFFICENCY OF ACTIVE PFC CONTROLLERS DROPS WITH OUTPUT LOAD. WHAT SUGGESTIONS CAN YOU ADVISE SO WE CAN LOWER THE HARMONICS.
WILL THE UCC28051 BE ABLE TO CONTROL THE HARMONICS DOWN TO THAT LEVEL OR SHOULD WE LOOK FOR ANOTHER CHIP USING A DIFFERNT PFC SCHEME
TONY
APX TECHNOLOGIES