Did a design using Webbench, it didn’t work as expected. I bought a LM25085 Eval board, it works great. So I figured I’d start with that design.
The documentation in the app note (AN1505 11/12/2008) does not match the PCB in the kit ( P/N 551600255-001 REV A 2008)
I tried calling the new support people but they said they really didn’t know National parts and to try here…..
The 100uf aluminum cap C1 in not in the documentation.
R7 appears to be a different value
47.5K on the board 23.2k on schematic
I can’t tell if the C’s are different as they are not marked
The Schottky is a dual type, are they in parallel?
Is there any way to get up to date documentation?