Is the automotive version the exact same chip but binned/tested at higher temps? I notice that the Q1 datasheet suggests the nominal maximum current be 60mA... is this only to meet the higher operating temps? I need both automotive and commercial application and so I am considering purchasing Q1 for both. But it would be nice if the commercial users could still run them at 80mA.
Also, I noticed that the G4 suffix supposedly means "green" but the web site claims the non G4 version is also ROHS. What is the difference?
Thanks!
Andrew